Your data collection solution uploads transaction data into the SyteLine data collection tables. Depending on options you set in the Data Collection Parameters form, the data is either automatically posted to the SyteLine database, or it remains in the error processing table until you manually validate and post the transactions through the appropriate Error Processing forms.
You can include jobs with co-product mixes in the data collection tables. By-products are not supported for data collection solutions.
To post and validate data collection transactions, use these steps:
NOTE: For transaction types that are set to Auto-Post and have background tasks defined through the Data Collection Parameters form, validated transactions are automatically posted to the appropriate SyteLine file, and the Post button is disabled on the Error Processing form. For these types of transactions, you can only view transactions that contain errors in the Error Processing forms. You can also check the Background Task History for problems that might have occurred during auto-posting.
When you post the transactions from the Error Processing form, the system defaults to the current date. Specify the date through which to post transactions or accept the displayed date.
NOTE: Transactions for items flagged obsolete or slow-moving may not post.
If a transaction has an Unposted status after posting is performed, but there is no error associated with it, the end time is within the Job Grace Period specified on the Data Collection Parameters form, and the transaction can still be adjusted.
On the Background Task Definitions form, you can see all of the available DCPost... tasks. Notice that they all have Concurrency set to 1, which means that only one instance of this task can run at a time. Do not change that setting, because it prevents different instances of the same background posting tasks from running simultaneously if you accidentally set the task run times to overlap.
To determine if a recurring data collection background task is set up to run, go to the Active Background Tasks form and look for these background tasks that are associated with the Auto-Post options:
| Post Option | Background Task |
| Auto-Post Receiving | DCPostPurchaseOrderReceiving |
| Auto-Post Shipping | DCPostCustomerOrderShipping |
| Auto-Post Cycle Count | DCPostCycleCounting |
| Auto-Post Misc Issue/Receipt Qty Adjust | DCPostMiscIssue/ReceiptandQuantityAdjust |
| Auto-Post Quantity Move | DCPostQuantityMove |
| Auto-Post Job Material | DCPostJobMaterial |
| Auto-Post Job Receipt | DCPostJobReceipt |
| Auto-Post Transfer Ship | DCPostTransferShip |
| Auto-Post Transfer Receipt | DCPostTransferReceipt |
| Auto-Post Mfg Labor | DCPostMfgLabor |
| Auto-Post Time/Attendance | DCPostTime/Attendance |
| Auto-Post Production Schedule | DCPostProductionSchedule |
| Auto-Post JIT | DCPostJIT |
| Auto-Post Work Center Material | DCPostWorkCenterMaterial |
NOTE: The Auto-Post Job Transactions option does not have its own background task, since it is used to turn on more processing for the Auto-Post Manufacturing Labor task.
To find out the times and dates when the task is scheduled to run, look at the SQL job in the database.
To stop auto-posting (temporarily or permanently):
About the Error Processing Forms
About Data Collection Transaction Validation
About Co-Products and By-Products