Maintaining Multi-Site Items from a Master Site
Use the Multi-Site 
 Items form to maintain items for multiple sites on an intranet from 
 the master 
 site of the intranet. Keep in mind that each site can still control 
 its local item records.
Adding Items
To add item for any site on the master site's intranet, follow the steps 
 in Creating a New Item. 
Copying Items to Other Sites
To copy an item to multiple sites in the same intranet from this form:
	- Select an existing item.  The item must be defined as completely 
	 as possible before you copy it, and the item record must be saved 
	 at one of the shared sites in the master site's intranet.
- Select Actions > Multi-Site 
	 Copy. The Multi-Site Selection 
	 form is displayed.
- Select one or more groups from the list of site groups in the left 
	 pane. The left pane only lists site groups where all of these are 
	 true: 
	
		- The site group includes the master site. 
- The site group includes the source site from which the selected 
		 record will be copied.
- All sites in the group are on the master site's intranet
 
- A list of the sites in those groups is displayed in the right pane. 
	 Select one or more sites to which you want to copy the item. 
- Click OK to return to the 
	 Multi-Site Items form.
- Save your changes to add the duplicate item records to the other 
	 sites.
Note: This procedure 
 does not copy the item's BOM. To copy an item's single-level current routing 
 and BOM to the same item at other sites, see Copying 
 a Multi-Site Item Bill of Materials.
Information Filtered by Site
You specify the site when you add an item. The following fields are 
 filtered by the selected site. For example, when you add an item and specify 
 Site B, you can only select product codes that are valid at Site B.
	- Alternate Item
- U/M
- Product Code
- Unit Weight U/M
- Family Code
- Production Type
- Warehouse
- Setup Group
- Reason
- Backflush Location
- Preferred Co-product Mix
- Commodity
- Origin
The Buyer field is filtered by the master site. That is, the information 
 in the drop-down list is from the master site, not the site you specified.
Maintenance Tasks Not Available from this Form
For most tasks, you can use the Multi-Site Items form in place 
 of the Items form. However, these tasks can be performed only in 
 the Items form at the specific site:
	- Delete an item
- Add notes to the record
- Specify tax information
- Define item categories, attributes, and related items
- Provide a picture of the item
- Display the BOM view
- Define scheduler batches for the item, and set a few other APS-related 
	 options
- Use Actions menu "List" options
Related Topics
Multi-Site 
 Overview
Adding a Multi-Site 
 Item (No Master Site)