Copying a Multi-Site Item Bill of Materials
Use the Multi-Site Bill of Materials 
 Builder to copy an item's bill of materials (BOM) from this site 
 to all selected sites.
To copy an item's BOM:
	- Specify the item to be copied. The description, type, and source 
	 information for the selected item is displayed. 
- Explore the current BOM tree for the selected item, which is displayed. 
	 To explore the BOM, you can right-click and launch the appropriate 
	 form from the tree for items and operations. However, the tree is 
	 not recursive, so you cannot drill down to jobs. 
	Note: Verify 
	 that the records listed in Validations, below, exist in the 
	 target site and match the values defined in the BOM.  
- Select Create Non-Inventory Items 
	 to create in the target site any non-inventory items that are included 
	 in the BOM. (Inventory items must already be defined in the target 
	 site before you perform the copy.) For more information, see About 
	 Non-Inventory Items and Managing 
	 Non-Inventory Items.
- Select the target sites in the grid to which you want to copy the 
	 BOM. To select or deselect all listed sites, use the buttons.
- Click Copy BOM. A confirmation 
	 message box is displayed if the copy was successful.  If the 
	 copy failed at any of the sites, a message that indicates the error 
	 is displayed next to the site in the grid, and the copy is rolled 
	 back at that site. The process then continues to the next site.  If 
	 the copy to a site failed because of a validation error, see Validations, below, for more information. 
	 
Rules for Using the Builder
	- The item must already exist in the sites to which you plan to copy 
	 the item's BOM.  To copy the item to the other sites, see Maintaining Multi-Site Items 
	 from a Master Site or Adding 
	 a Multi-Site (Global) Item (No Master Site).
- If a BOM for the item already exists in the selected site, then 
	 the existing BOM is deleted before the new BOM is copied to the site. 
	 
- Standard BOMs cannot be copied.
- The Builder copies a single level at a time. To create a complete 
	 indented BOM in the other sites, you must copy each of the manufactured 
	 components (individual levels of the BOM) separately, as well as all 
	 phantom items 
	 separately. Copy all of this information to each of the sites where 
	 you are copying the item’s BOM.
- If the item whose BOM is to be copied is revision-tracked in the 
	 target site, then a message is returned and the BOM is not copied.
Replication Notes
A replication rule must exist between the source and target sites that 
 specifies the Multi-Site BOM Builder replication category.
We recommend that this process only be used with transactional replication. 
 If a validation fails during transactional replication, a message is displayed 
 and the whole process is rolled back. The Builder also works with non-transactional 
 replication; however, if a validation fails in the middle of the process 
 during non-transactional replication, it could leave the target site in 
 an error state. For example, the target site’s current BOM was deleted 
 but only part of the new BOM was created.
Validations
Certain fields are validated to ensure that they already exist in the 
 target site before the BOM is copied. If they do not exist, a message 
 is displayed and the BOM copy could fail and be rolled back.  The 
 existence of these records is validated in the target site:
	- When Current Operations are copied: 
	
		- Parent Item 
- Work Center 
- Setup Matrix 
- Work Center Setup Time Rule 
- Scheduler Rule 
- Batch Definition 
 
- When Current Materials are copied: 
	
		- Parent Item 
- Component’s Operation 
- Component Item 
- U/M Conversion to this U/M 
- Component Manufacturer ID 
- Component Manufacturer Item 
- Component Feature 
 
- When Resource Groups are copied: 
	
		- Parent Item 
- Resource Group 
 
- When Reference Designators are copied: 
	
		- Component Item 
- Component Operation number 
 
- When Product Configuration Features are copied: 
	
		- Component Item 
- Component Operation number 
 
Note: It is your 
 responsibility to manually verify that the values match in both sites 
 before the copy is performed. For example, if item BS-100 is defined as 
 a bike seat in the source site and item BS-100 is defined as a tire in 
 the target site, the Builder will  copy the routing and materials 
 to build a bike seat to the tire item in the target site. 
Related Topics
Maintaining 
 Multi-Site Items from a Master Site
Adding 
 a Multi-Site (Global) Item (No Master Site)
About 
 Non-Inventory Items