NOTE: See Writing a Custom Scheduler Rule for a summary of the steps required to create custom rules. For more details about the functions described in this topic, see the Simulation Tailoring Support Function Reference (available for download from the Support web site, on the documentation page for the Infor APS Virtual Planning/Simulation product).
To determine whether a setup is necessary, you can write a function, ucwtsr, that the Scheduler uses when the Setup Rule on an operation is set to a user-defined setup rule (rule positions 3-39).
Your custom function can have any name that is not a standard user-callable function name.
#include "factor.h" int ucwtsr (ldp, type, rp, jsp, rule) LOAD *ldp; /* pointer to the load. */ TCHAR type; /* 'R' (resource) */ void *rp; /* pointer to the resource to setup. */ JOBSTEP *jsp; /* pointer to the operation. */ int rule; /* setup rule to use. */
Function ucwtsr must accept five arguments in the following order:
The function should return 1 for success (setup should be done) and 0 for failure (setup should not be done). Type: int.
The following example of ucwtsr sets up a resource every time the part and/or operation changes for the resources.
int ucwtsr(LOAD *ldp, TCHAR type, void *rp, JOBSTEP *jsp, int rule)
/*-----------------------------------------------------------------
Function to set up a resource if the item or operation is
different from last setup
ARGS:
ldp - pointer to load
type - "R"esource
rp - pointer to resource
jsp - pointer to operation
rule - Setup rule
RETURNS
true - perform setup, or
false - do not perform setup
-----------------------------------------------------------------*/
{
int ireturn = 0
char error[400];
/* Check if setup or setup/operate or super operation. */
if ( (jsp->jstype != 4) && (jsp->jstype != 13) )&&
(jsp->jstype != 19) )
{
sprintf(error,"Operation not a Setup or Setup/Operate or Super
operation\n\nOrder ID %s\nLoad ID %d\nBatch ID
%ld\nOperation ID %s\nOperation Type %d\n",
ldp->loordp->orid, ldp->loid, (ldp->lobat == NULL)
? OL : ldp->lobat->bibatid, jsp->jsid, jsp->jstype);
seferr(0, error);
}
if (type == 'R')
{
ireturn = (((RESRC *)rp)->rsptst != ldp->loordp->orptpt
|| ((RESRC *)rp)->rsjsst != jsp) ? 1 : 0;
}
else
{
ireturn = (((MCRMEMBER *)rp)->mbrptst != ldp->loordp->orptpt
|| ((MCRMEMBER *) rp)->mbrjsst != jsp) ? 1 : 0;
}
return (ireturn);
}
It is not necessary to install ucwtsr in ucini1 because it is called automatically when the setup rule is greater than 2 (that is, a non-standard rule number).
Compiling and Linking Custom Scheduler Rules