Setting Up the Euro Currency Code
To enter the currency code for the Euro currency on 
 the Currency Codes and Currency Rates forms, follow these 
 steps:
	- On the Countries 
	 form, add a new country code for the European Economic and Monetary 
	 Union (or whatever you want to call the country code that will be 
	 associated with the Euro in your system).
- Access the Currency 
	 Codes form.
- Select New from the Actions menu.
- In the Currency field, enter the code to represent the Euro, such 
	 as ECU.
- In the Description field, enter descriptive text for the Euro currency 
	 code.
- In the Currency Symbol field, enter the characters to display with 
	 the currency. The default value is the same as the currency code (you 
	 can overwrite it).
- Save the record.
- Access the Currency 
	 Rates form.
- In the Buying and Selling Exchange Rate fields, enter the number 
	 of Euros equal to one unit of your domestic national currency.
- In the Effective Date field, enter the date on which you are adding 
	 the Euro as a valid currency code in your system.
- Save the record.
- On the Multi-Currency 
	 Parameters form, enter the Euro currency code in the Euro Currency 
	 field.
Specifying the Euro as Your Domestic Currency
When you create the database, you can specify the 
 site (domestic) currency as the Euro. Otherwise, if you want to convert 
 your domestic currency from another currency to the Euro, you must use 
 the Domestic 
 Euro Currency Conversion utility to change the domestic currency 
 to the Euro and convert all related records.
Related Topics
Euro Currency 
 Overview
Customer 
 Euro Currency Conversion
Domestic 
 Euro Currency Conversion
Euro 
 Exchange Rate Revaluation
Vendor 
 Euro Currency Conversion