The Executive Home form displays a variety of data that helps executive management perform their jobs. This form is not part of a permission group. Authorization must be specifically given through the Object Authorizations for User form.
Use the Multi-Site Group field to select which site group will be displayed on this form. All sites in the selected group will be represented in the tabs.
When viewing a tab on this form, if a small Earth icon displays in the upper left corner, then the data on that tab can be compiled from multiple sites. Data on a tab with the Earth icon can still only be single site data, but if the Earth icon is on that tab, then that means that tab has the ability to display multi-site data. If no icon displays, then the data on that tab is from the current site. When viewing data from multiple sites, no right-click menu is available.
The following buttons, which appear on the upper portion of this form, can be used to quickly open complementary applications. If an application is not installed, its button is inactive.
For information about the tabs on this form, see these topics: