Monitored Resources

Use this form to monitor any Windows service or resource, such as disk space. When the system is monitoring a resource, and a certain event occurs in relation to the resource (for example, low disk space), the system can send alerts to a mobile device, or e-mail notifications. In order to receive these alerts or e-mails, the SyteLine users must be subscribed (in the Publication Subscribers form) to the publication that sends the alert.

Alerts are sent to the subscribers' e-mail or phone address, if it is specified on the Publication Subscribers form. If no e-mail or phone address has been specified, alerts are sent to the user's SyteLine inbox.

NOTES:

Related Topics

Monitoring Disk Space

Setting Up to Kill Long-Running Tasks

Monitoring a Service

Setting Up Mobile Access