Monitoring a Service
To monitor a Windows service:
	- In the Windows Services window, right-click on the service and 
	 select Properties to find 
	 the official Service name.
 
	- In the Publications form, 
	 create a publication for the alert  with at least one subscriber. 
	 Subscribers to this publication will receive an alert when the service 
	 is stopped.
 
	- In the Monitored 
	 Resources form, specify this information for the service: 
	 
	
		- Resource Type: Service
 
		- Resource Name: The name you found in Step 1
 
		- Machine Name: Name of the utility server where the service 
		 runs 
 
		- User Name / Password: Windows Administrator user name and password 
		 to connect to that server 
 
		- Domain: Domain name of that server 
 
		- Alert Subject: Brief description of the reason for the alert, 
		 for example: [xxx] service on [servername] is stopped. 
 
		- Alert Message: Message that is sent to the user.
 
	
 
	- In the Publication field on the Monitored Resources 
	 form, select the publication you specified in Step 2.  This associates 
	 the alert with the publication.
 
	- To verify that the monitor is working, go to the Status tab and 
	 click the Status button. You 
	 should see a response in the Status field.
 
	- Select Active so the Application 
	 Event System will monitor this service and send subscribers an alert 
	 when the service stops.
 
Related Topics
Setting Up 
 SyteLine Mobile Access
Monitoring Disk 
 Space
Setting 
 Up to Kill Long Running Tasks