Details of Domestic Currency-to-Euro Conversion
Use the Domestic
Euro Currency Conversion utility to convert your base domestic currency
to the Euro (including all monetary amounts, exchange rates, and history
records). When you run this utility, the system does the following:
- Sets the Buying and Selling Exchange Rate fields to 1 for the Euro
currency record on the Currency
Rates form.
- Updates the Effective Date to today's date for all Part of Euro foreign
currency records on the Currency Rates form.
- Changes the Domestic Currency field on the Multi-Currency
Parameters form to the Euro.
- Updates the General Ledger.
- If a ledger record's currency code is your
old domestic currency, the utility converts the domestic and foreign
amounts using the standard currency conversion, sets the exchange
rate to 1, and sets the currency code to the Euro.
- If a ledger record's currency code is the
Euro, the utility sets the domestic amount equal to the foreign amount
and sets the exchange rate to 1. The currency code and the foreign
amount remain the same.
- The utility accumulates the total debits
and credits for pre- and post-conversion amounts for each distribution
journal and ledger.
- Converts exchange rates and amount values in the following areas:
- Distribution journals
- General Ledger
- Customer-related records
- Vendor-related records
- Transfers
- Jobs
- Work Centers
- Inventory
- Human Resources
- Fixed Assets
- Project Costing
- Other miscellaneous records
Conversion Notes:
- The values for some fields are calculated from other fields (for
example, Brokerage + Duty + Freight + Insurance + Local Freight +
Material = Item Cost). The system does not convert these fields directly;
instead, it recalculates them after their component fields' values
are converted.
- The system converts unit of measure fields using the standard processes
maintained on the Unit
of Measure Conversions form.
- If a record contains an amount in a foreign currency and the record's
currency code is the Euro, the utility sets the domestic amount equal
to the foreign amount and sets the exchange rate to 1. (This practice
reduces rounding variances.)
- See Unconverted
Records for a list of the types of records this utility
does not convert.
Related Topics
Euro Currency
Overview
Converting
the Domestic Currency to the euro
Customer
Euro Currency Conversion
Euro
Exchange Rate Revaluation
Vendor
Euro Currency Conversion