This topic describes how the system handles the Euro currency. It does not attempt to describe the details of the Euro currency system or any related rules and regulations.
For Euro-participating countries, there may be an interim period during which the country is converting their national currency to the Euro currency. During this interim period, financial transactions between participating countries can be completed in either the Euro currency or the national currency.
If you are a Euro participant, the system performs the necessary currency conversions when you conduct transactions with other Euro-participating countries during the interim period. When you change your domestic currency to the Euro, you can use the system utilities to convert all of your relevant business history. If you are not a Euro participant, but you conduct transactions with Euro-participating countries, the system performs the currency conversions.
When you are ready to switch to the Euro, the Domestic Euro Currency Conversion utility converts your base domestic currency. The utility converts all domestic currency-specific amounts, including history data.
If any of your vendors have switched to the Euro, you can use the Vendor Euro Currency Conversion utility to convert all transaction amounts stored in the vendor's old currency. Similarly, the Customer Euro Currency Conversion utility allows you to convert any customer transaction amounts stored in the customer's old currency.
All accounts receivable, accounts payable, and vouchers payable records in the system are expressed in the transaction currency of the customer or vendor. These records also contain an exchange rate to translate the values back to your base currency. As of 1/1/1999, the exchange rate between Euro-participating currencies and the Euro currency is fixed.
Therefore, you must revalue outstanding assets and liabilities using the fixed exchange rate. Run the Currency Revaluation utility, the Bank Account Revaluation utility, and the Euro Exchange Rate Revaluation utility.
The system allows you to accept payments in either the customer's transaction currency, the Euro currency, or your base domestic currency. During the interim period, you can accept payments in the Euro currency without switching your base domestic currency to the Euro. Therefore, you can accept payments in the Euro currency only for those transactions that require it, and deposit the customer payments in a base or Euro bank account.
The following system reports allow you to print the total monetary amount in both the Euro currency and the transaction currency for any Euro-participating customer or vendor:
Invoices, Debit and Credit Memos
Accepting Customer Payments in the euro Currency
Converting Customer Records to the Euro
Converting Vendor Records to the Euro
Converting the Domestic Currency to the euro
Revaluing Assets and Liabilities for the Euro
Setting Up the Euro Currency Code
About the euro Triangulation Conversion
Customer Euro Currency Conversion
Customer Orders and Invoices in Foreign Currencies
Domestic Euro Currency Conversion