The system provides several different types of auditing:
NOTE: We strongly recommend that you enable audit logging only if there is a specific need to check something, and enable it for only a short time. The audit trail processing is extensive and robust. While enabled, it will reduce system performance and create a large number of process records in the log.
Material Transaction (matltran) records provide an audit trail for material transactions. Material transactions are created when you:
You can print this audit trail with the Material Transactions Report.
Use the Delete Material Transactions utility to delete most types of material transactions, except End of Period Costing transactions. End of Period Costing transactions include Just-In-Time (JIT) Production Transactions, Production Schedule Complete Transactions, Production Schedule Scrap Transactions, Work Center Labor Transactions, Work Center Machine Time Transactions, and Work Center Material Transactions. You can run Delete End of Period Costing Transactions to delete End of Period Costing transactions.
CAUTION: Be sure to run the Material Transactions Report before you delete any material transactions, to preserve the audit trail. When a material transaction is deleted, references to that transaction from any ledger or journal records will be cleared. If you then try to view detail on a ledger or journal previously referenced to the deleted material transaction record, the system will display a message saying that the record is not available.
Prior to posting inventory cycle counts, run the Cycle Count Variance Report to provide an accounting audit trail for any variances encountered from the original quantities.
Before using the Physical Inventory Count Posting utility to post inventory quantities to the Quantity On-Hand field, we recommend you run the Preadjustment Report to generate an accounting audit trail for visibility for count discrepancies.
For a description of the differences between cycle counts and physical inventories, see Differences Between Cycle Counts and Physical Inventories.
Use the Physical Inventory Records Purge utility to erase the contents of the Physical Inventory files once the entire physical inventory is approved and posted, and the auditors have reviewed and approved the results. The purpose of this option is to release disk space taken up by the Physical Inventory file. Although the contents of the file are erased, an audit trail of the Physical Inventory posting is still available. The Item/Warehouse file contains these fields for reference purposes: Physical Inventory Count (quantity counted)and Physical Inventory Date (date the posting occurred).
Job Transaction (jobtran) records provide an audit trail for labor transactions (job, production schedule, JIT, and work center). You insert Job Transaction records into the jobtran file manually and use the Job Labor Transaction Posting feature to post them. Be sure to run the Job Transactions Report before you delete any job transactions, to preserve the audit trail. You can delete this type of record only by using the Delete Job Transactions utility.
Before posting invoices, debit memos, and credit memos through the Invoice Posting activity, print the Invoice Transaction Report as an audit trail of the posted items.
A/R Draft Purge deletes canceled, paid, and voided drafts. It produces a register of the purged drafts as an audit trail.
Before posting A/P voucher and adjustment transactions, print the Voucher Transaction Report as an audit trail.
Before using the Mass Journal Posting utility or the Ledger Posting for Journal utility to post transactions from one or more journals to the ledger, print the Journal Transaction Report as an audit trail of the items that will be posted. Also, before using Journal Compress to reduce the number of transactions in a journal, you must print the Journal Transaction Report.
On the Direct Deposit Banks form, enter the General Ledger account number that will be credited and debited when a direct deposit is posted for an employee using this bank. This account maintains an audit trail of direct deposits to the bank.
When you set up Project Parameters for revenue milestones and invoice milestones, you can enable audit trails. The audit information then appears in an Audit tab on the Revenue Milestones, Estimate Revenue Milestones, and Invoice Milestones forms.