Project Manager Home

The Project Manager Home form provides a wide variety of information from other parts of the system in one form, all intended to be used by a project manager. This form is not part of a permission group. To get access to this form, your system administrator must give you authorization for this form.

Multi-Site

When viewing a tab on this form, if a small Earth icon displays in the upper left corner, then the data on that tab can be compiled from multiple sites. Data on a tab with the Earth icon can still only be single site data, but if the Earth icon is on that tab, then that means that tab has the ability to display multi-site data. If no icon displays, then the data on that tab is from the current site. When viewing data from multiple sites, the right-click menu contains only 'Help'.

If you plan to view multi-site data on this home form, you must create a replication rule between sites that includes the replication category Multi-Site Project Manager.

Buttons

The buttons that are displayed on the upper portion of this form can be used to quickly open complementary applications. If an application is not installed, its button is inactive.

Tabs

For information about the tabs on this form, see these topics:


Related Topics

About Critical Numbers

About DataViews