Debugging Tax Calculations (Taxware)

If you are using the Taxware tax interface, you can use Debug fields on the Tax Interface Parameters form to help find and correct problems with your tax interface calculations.

Note: Do not turn on the debug options unless you have a problem with the interface.  When debugging is turned on, large amounts of data are written to the database, which can affect system performance.

To set up debugging of your tax interface:

  1. In the Tax Interface Parameters form, select a debug option:
  2. Save your changes on the form. At this point, the system starts logging any relevant information as users perform actions that involve tax calculations.
  3. When you have a good sample of transactions involving taxation, send the file to Support:
  4. If you are using the Debug Infor option, click Delete All to remove the debug log entries from the database after they have been exported to the file.
  5. Clear the Debug Infor and/or Debug Taxware option to stop logging entries.

Related Topics

About the Tax Interface

Setting up a Taxware Tax Interface