A Team transaction is defined as a group of two or more employees working on a single job at one machine. A team’s members are dynamic, meaning that the administrator is not required to predefine the team members.
Prior to using the Team transaction option in Shop-Trak Shop Floor, go to the Shop-Trak Teams form and specify a particular work center as one that uses a team. For the purpose of Shop-Trak, the definition of Team is limited to a fixed or variable crew of employees working in one work center. The Team ID is limited to that particular work center. If members of the team transition from one work center to another in the course of daily work, an additional Team ID can be set up or the employee can punch into another job which does not require a team.
NOTE: Multiple Team IDs for any given work center may be required to aid in the transition of shifts. For example, the members of the second shift team arrive and punch in before the first shift team members have punched out. The Shift Field on the Shop-Trak Teams form is for display only to assist in setting up these transitional Team IDs.
The full labor hours of each employee with full manufacturing rate and full overhead is applied to the job.
Bob, Fred, and Bill are on a team. Bob is the Team Leader. Each of their manufacturing rates is $15 per hour. The overhead for the department they are working in is $10 per hour.

Team Transaction Costing |
||||
Employee |
Labor Hours |
Labor Cost ($15/hr) |
Overhead Cost ($10/hr) |
Total Cost |
Bob |
3 |
$45 |
$30 |
$75 |
Fred |
2 |
$30 |
$20 |
$50 |
Bill |
2 |
$30 |
$20 |
$50 |
Jim |
2 |
$30 |
$20 |
$50 |
Total |
9 |
$135 |
$90 |
$225 |
Shop-Trak Defining Main Parameters
Shop-Trak Defining Flags Parameters