Shop-Trak Reviewing Pending Inventory & Material Transactions
JIT, Job Material, Production Schedule Complete/Scrap, and Work Center
Material transactions created in Shop-Trak Shop Floor transfer and post
directly to Infor SyteLine using the
Infor Framework TaskMan service. These transaction types
do not use the Shop-Trak Background Polling process. Any inventory
and material transactions that do not
post successfully are held in
the following Shop-Trak activity forms. Any inventory and material
transactions designated to not
post automatically are also held
in these forms (refer to Defining Background
Parameters for more information).
- Shop-Trak Pending JIT Transactions
- Shop-Trak Pending Job Material
Transactions
- Shop-Trak Pending Prod Sched Transactions
- Shop-Trak Pending Work Center
Transactions
Setting Up E-mail Notification of Posting Errors
Using the SyteLine Event Handler System, the Administrator can set up
e-mail notification for material and inventory transactions that did not
post successfully:
- Open the Event Global Constants
form.
- Filter the Name field for
ShopTrakAdminID.
- In the Value field, specify
the User ID (from the Users form) of the SyteLine user
that will be receiving the e-mail notification. Multiple User
IDs can be listed, separated by a semi-colon.
- Verify that a valid Primary E-mail
Address is entered on the E-mail
Address tab of the Users
form.
- If the transaction fails to post, the user specified above will
receive an e-mail containing the Transaction Type, Serial Number,
Status, and Item Number of the transaction.
Reviewing and Resubmitting Pending Inventory & Material Transactions
To review and resubmit pending inventory and material transactions:
- Open the Shop-Trak pending transactions form for the transaction
type that did not post.
- Information for the pending transactions displays as read-only.
Each form will include some combination of the following fields
on the Detail tab:
- Acct - Account numbers
associated with the transaction.
- BG Task Number - TaskMan
background processing number.
- Job material check boxes -
Additional information pertaining to the Job, Material,
or Serial Number will be checked. If the material is serial
tracked, the serial number will be listed on the Serial
Number tab.
- Container - Container
number.
- Cost - Material cost.
- Description - Item
description.
- Employee - Employee
number of the employee that performed the transaction.
- Error - Contains the
error message. If TaskMan is not running, the Error
field will be blank.
- Item - Item identifier.
- Job - Job number.
- Job Lot - Preassigned
lot number of the job item.
- Job Serial Number -
Preassigned serial number of the job item.
- Loc - Stock location
that the material will be moved to or issued from.
- Lot - Lot number associated
with the transaction.
- Oper Num - Job operation
number.
- Processed - Indicates
whether or not the transaction processed. If Errored
is displayed, the transaction tried to post but could not due
to an error condition. If No
is displayed, the transaction did not post because TaskMan is
not running, or its Post Pending Inventory and Material Transactions
check box is disabled on the Background
tab of the Shop-Trak Parameters
form.
- Qty or Quantity
Complete - Quantity to move to or issue from inventory.
- Quantity Scrapped -
Quantity scrapped.
- Reason Code - Code
and description of why the material was scrapped.
- Schedule ID - Production
Schedule ID.
- Sequence - Material
sequence from the Job Bill of Materials.
- Shift - Shift identifier
of the employee that performed the transaction.
- Transaction Date -
Date and time the transaction occurred.
- UM - Unit of
Measure.
- WC - Work Center.
- Whse - Warehouse to
which the material is to be issued or withdrawn from.
- Work Date - Date the
employee performed the transaction.
- Review the Processed
and Error fields to identify
the reason the transaction did not post.
- The
Serial Numbers tab will display serial numbers for any serial
tracked material associated with the transaction.
- The
Backflush Lots
tab displays the lot information associated with the transaction.
- The
Backflush Serials
tab displays the serial number information associated with the transaction.
- Make the corrections needed in Infor
SyteLine to resolve the error.
- Ensure that TaskMan is running before
resubmitting.
- Click Resubmit.
- If the error condition cannot
be resolved, delete the record from the pending transactions form.
Re-enter the transaction in Shop-Trak Shop Floor.
Related Topics
Shop-Trak Pending
JIT Transactions Form
Shop-Trak Pending
Job Material Transactions Form
Shop-Trak
Pending Prod Sched Transactions Form
Shop-Trak
Pending Work Center Transactions Form
Shop-Trak Transaction Flow Chart
Shop-Trak Transaction Flow Overview
Shop-Trak
Backflushing of Lots & Serials Overview