Shop-Trak Customizing the Visual Dispatch
Using a special Administrative password protected login, Administrators
can customize certain attributes of the Visual Dispatch and save them
as the default for the Site or the Resource Group.
IMPORTANT:
You must have System Administrator (SA) access in order to set the
Visual Dispatch password.
Customization Levels
There are four levels of customizations
for the Visual Dispatch:
- Vendor Default
- Standard Visual Dispatch default (lowest level).
- Site - Default for the
Site, unless there is a Resource Group level, or a User Level (higher
level).
- Resource Group - Default
for the Resource Group, unless there is a User Level (higher level).
- User - Specific to the
employee login and will always be the default for the employee when
one exists (highest level).
Creating Site and Resource Group Customizations
To make and save customizations
at the Site and Resource Group level, a password needs to be set up for
the Shop-Trak Shop Floor Administrative login.
- From the Shop-Trak Utilities
menu select the Shop-Trak
Visual Dispatch Settings form.
- Specify an Admin
Password that will allow Administrators to log in to Shop-Trak
Shop Floor and customize the Visual Dispatch. There
are no minimum requirements for the password. At
any time, the password can be reset by opening this form and entering
a new password.
- Save the change and close the form.
Making Changes to the Visual Dispatch
- Open a Shop-Trak Shop Floor session and specify VisDisAdmin
in the Employee
field.
- Enter the Password that
was specified in the Shop-Trak Visual
Dispatch Settings form.
- In the Identify Your Editing Scope
window, specify at what level the changes are applicable: To the Site or the
Resource Group.
- When the Visual Dispatch opens, it will be empty.
- From the Resource Group
drop-down, select a group to make the changes for. If the
changes are Site level, any
Resource Group may be selected.
- The following attributes can be changed:
- Column Order –
Put the most referenced columns to the left. Least
referenced information can stay off to the right. To
move a column, simply select the column and drag it to the column
location and release to insert the column.
- Column Width –
The column width is set to a default value. Change
the column width to suit the data being displayed.
- Row Height – Adjust
the height of the rows to show more or less information.
- Splitter Position
– Drag the splitter between the upper grid and the lower grid
to show more or less on the top or bottom.
- Tab Color – Right-click
on each of the tabs. A
color menu will display. Set
the colors of the tab to best suit the desired look and feel.
- Notice at the bottom of the form, the Editing
Level is displayed for reference.
- When all changes are made, click Send
to save the changes:
- Click Save to keep
the changes.
- Click Cancel to ignore
any changes made and close the form.
- Once changes have been made and saved,
the next time the Administrator logs in and makes changes, the option
to revert to the Default Settings will be available. Choosing
this option will discard all changes and bring back the original form.
Related Topics
Shop-Trak Defining
Main Parameters
Shop-Trak
Setting Up the Employee Profile - Options Tab