Shop-Trak Setting Up the Employee Profile - Options Tab
Use the Options tab of the Shop-Trak Employee Profile form
to enable or disable functions such as reporting quantities and closing
job operations. You can also use this tab to designate approvers
and set up employee defaults.
To set up Options for an employee:
- Open the Shop-Trak Employee Profile
form.
- Click the Options tab.
- Specify this information:
Functions
- Disable Qty
Complete - Select this check box to prohibit the entry
of completed quantities by the employee. If the employee
is designated as an RTE Employee on
the General tab, this field will be checked by default.
- Disable Qty
Scrapped - Select this check box to prohibit the entry
of scrapped quantities by the employee. If the employee
is designated as an RTE Employee on
the General tab, this field will be checked by default.
- Disable Operation/Job Complete
- Select this check box to prohibit the completion of a job or
operation by the employee when ending a transaction. If
the employee is designated as an RTE
Employee on the General tab, this field will be checked by default.
- RTE Transaction Confirmation Required
- This option only applies to RTE employees.
Select this check box to require RTE
employees to confirm their transactions at the end of the week.
When they log in to Shop-Trak Shop Floor, a Confirm button will display.
After clicking Confirm,
the RTE
Weekly Confirmation screen displays.
Visual Dispatch
- Auto-Launch Dispatch
- Select this check box to allow the employee to start and end
Run, Setup, and Direct transactions from the Visual Dispatch screen.
After entering an employee ID, selecting a transaction type,
and clicking Send, the
Visual Dispatch screen
will auto-launch and display jobs for the employee’s Default Resource
Group. The employee then selects the desired job and clicks
Send to begin the transaction.
- Allow Save to Visual Dispatch
- Select this check box to allow the employee to save any of the
following changes made to the Visual Dispatch screen:
- Column width
- Column order
- Row height
- Splitter position
Once the employee saves the changes, these
settings will override any made at the Resource Group, Site Default, and
Vendor Default levels.
Approving Supervisors
The Approving Supervisors
section defines the employee's Primary, Alternate, and Admin
Supervisors, mainly for transaction approval purposes. Designated
supervisors are also used as selection criteria on the Shop-Trak Time
& Attendance/Delinquency Report and other Shop-Trak reports.
- Primary - Select
the employee's Primary Supervisor.
- Alternate - Select
the employee's Alternate (Secondary) Supervisor. The Alternate
Supervisor will approve the employee's transactions in the absence
of the Primary Supervisor.
- Admin
- Select the employee's Administrative Supervisor. The Administrative
Supervisor will approve the employee's transactions in the absence
of the Primary and Alternate Supervisors. An example of
an Administrative Supervisor would the be the staff member responsible
for Payroll. The Payroll staff member needs the ability
to make sure all transactions are posted before payroll is generated.
In the event the Supervisors are absent, the Payroll staff
member can approve the employee's transactions.
- Require Transaction Approval
- Select this check box
to require approval of the employee's transactions by an Approving
Supervisor before the transactions transfer to Infor SyteLine.
NOTE:
The supervisor assignments will not qualify the supervisors to override
or log the employee in on a biometric device. The supervisors assigned
on this form are only permitted to approve the employee’s daily transactions
and run Shop-Trak reports. Please see the Biometric
Approver section of the Employee Profile
Biometric topic on how to designate an employee as a Biometric Approver.
Shift Options
- Flex Shift - Enabling
this option will display the available alternate shifts when the
employee logs in to Shop-Trak Shop Floor. To set up the
employee for alternate shifts:
- Select the Flex Shift
check box.
- Select the desired alternate shifts from the drop-down list
in the Shift grid.
NOTE: You must include the Employee Master Shift
as one of the shifts. If you do not, upon saving you will receive a message
stating "The Employee Master shift must be in list of available shifts
when 'Flex Shift' is enabled."
- When the employee signs in
to Shop-Trak Shop Floor, the available alternate shifts
will now display for selection. The Lunch and Break Schedule
and any shift premiums will be assigned according to the selected
shift. The selected alternate shift will only be applicable
for the current day.
- Clearing the Flex Shift check box removes the option for the
employee to select an alternate shift upon login. Instead,
the employee will automatically be assigned the default shift
from the Employee
Master Shift field. Note
that the selected alternate shifts remain in the Shift grid even
after the Flex Shift check box has been cleared.
- Employee Master Shift - This field displays
the default Shift
number from the Employees
form.
Employee Defaults
These parameters are optional.
- Vis
Disp Resource Grp - Select the default Visual
Dispatch Resource Group to display when the employee accesses
Visual Dispatch. This Resource Group will remain as
the default unless the employee selects a different Resource Group.
If the employee changes the Resource Group, the new selection
becomes the default for the remainder of the day, or until changed
again. When the employee begins a new day, the initial default
Resource Group becomes the primary selection once again.
- Vis Disp
Resource - Select the default Visual
Dispatch Resource to display when the employee accesses
the Visual Dispatch screen.
This Resource will remain as the default unless the employee
selects a different Resource. If the employee changes the
Resource, the new selection becomes the default for the remainder
of the day, or until changed again. When the employee begins
a new day, the default Resource becomes the primary selection
once again.
- Default Ind
Code - Select the Indirect
Code to use as the default when the employee starts an
Indirect transaction.
NOTE:
There may be cases where not all the available Indirect Codes
appear in the drop-down list. Indirect Codes that are assigned
to Breaks or Lunches on the Shop-Trak
Break Lunch Schedule form are not available for use on the
shop floor. If an Indirect Code is manually entered into this
field and is used on a Break Lunch Schedule, a message displays
stating that the Indirect Code entered is invalid.
- Allow Default Ind. Code Only - Select this check box to
display the default Indirect
Code only. The employee will not be allowed to change
the code. Clear the check box to permit the employee to
change the code.
- Save the changes and close the form.
Related Topics
Shop-Trak Employee
Profile Form
Shop-Trak Setting up the Employee
Profile - General Tab
Shop-Trak Customizing the
Visual Dispatch