WinStudio
Form components with the data type DECIMAL.
Property defaults with the data type DECIMAL.
Component properties: Data type and format.
Specifies the minimum number of digits to the right of the decimal point.
DECIMALPOINT( integer )
Part |
Description |
| integer | Expression that evaluates to an integer specifying the minimum number of digits to the right of the decimal point. |
The DECIMALPOINT keyword affects only the visual format of values in WinStudio forms. With the specification DECIMALPOINT( n ), WinStudio appends zeros to the value of a component so the number of digits to the right of the decimal point is n. If the value does not have a decimal point, WinStudio appends a decimal point and n zeros to the right of it. If the value has at least n digits to the right of the decimal point, WinStudio does not change the value.
The DECIMALPOINT keyword can serve as a parameter of the DEFAULTFORMAT keyword in data-type specifications. See DEFAULTFORMAT, COMMA, and COMMAS in Related Topics.
A component value with the following format specification displays two digits to the right of the decimal point:
DEFAULTFORMAT(DECIMALPOINT(2))