WinStudio
Form components.
Extended data type variable values.
Property defaults.
Component property: Data type.
Specifies default format properties for the value of a component.
DEFAULTFORMAT( keyword( ) [keyword( ) . . .] )
Part |
Description |
| keyword( ) | Keywords and parameters that determine the visual format and other properties of the value of a component. The following keywords can serve as keyword() settings: |
WinStudio stores the DEFAULTFORMAT keyword, its parameters, and other specifications for a data type in a variable. If a default format is specified at the component level in the Form Component Properties dialog box, WinStudio creates a form-level variable whose name consists of the prefix dt_ and the name of the component with which it is associated. An extended data type variable is global, and the variable name consists of the prefix edt_ and the name of the user-defined data type on which it is based. Once you specify a data type, you can apply it, including DEFAULTFORMAT specifications, to a component by means of the variable.
In the following example of a data type specification, the DEFAULTFORMAT keyword sets the typeface to bold Times New Roman in blue.
DATATYPE(CHAR) DEFAULTFORMAT(FONT(-11,0,0,0,700,0,0,0,0,3,2,1,18,Times New Roman) FORECOLOR(0,0,255))