WinStudio
Form components with the data type DATE.
Property defaults with the data type DATE.
Component properties: Data type and format.
Specifies that the value of a component with the DATE data type consists only of a time of day.
TIME( )
A component with the DATE data type can parse, validate, and display both date and time user input. The TIME keyword specifies that the component contains only a time of day. With TIME specified, the value of a component returned by a script is a time, although the property to which the component is bound may contain both a date and a time.
The keyword can serve as a parameter of the DEFAULTFORMAT keyword in data-type specifications. See DEFAULTFORMAT, DATE, and DATETIME in Related Topics.
With the following data-type specification, a component displays only a time, and it parses and validates only the time portion of user input.
DATATYPE(DATE) DEFAULTFORMAT(TIME())