WinStudio
IWSFormComponent interface, grid objects
Assigns background and foreground colors to specified grid cells. This method uses integers to specify the cell locations.
For more information about background and foreground colors, see the "Remarks" section.
object.SetGridRowColColor( integer1, integer2, string1, string2 )
Part |
Description |
| object | Required. A reference to a grid object. |
| integer1 | Required. Indicates the row number.
Row numbering is 1-based. |
| integer2 | Required. Indicates the column number.
Column numbering is 1-based. If you use 0 (zero) for this value, the colors are applied to the entire row. |
| string1 | Required. A string containing the RGB code value of the color to be used for the background. |
| string2 | Required. A string containing the RGB code value of the color to be used for the foreground. |
The background color is used for the background color of the designated cells. The term "foreground color" typically refers to the font/text color.
The RGB strings consist of a series of three comma-separated integers, each in the range 0–255. For example, the RGB code for a deep purple color might be rendered as (158,44,186).
The use of an empty (null) string ("") tells the system to use the default setting for that value.
'The following code sets the background color to red
'and resets the foreground color to the current WinStudio default.
ThisForm.Components("FormCollectionGrid").SetGridRowColColor(5, 1, "255,0,0", "")
SetGridRowColColorByColumnName Method
SetGridRowColFontByColumnName Method
SetGridRowColImageByColumnName Method