WinStudio
IWSFormComponent interface, grid objects
Assigns background and foreground colors to specified grid cells. This method uses an integer to identify the row number and the column name to identify the column location.
For more information about background and foreground colors, see the "Remarks" section.
object.SetGridRowColColor( integer, string1, string2, string3 )
Part |
Description |
| object | Required. A reference to a grid object. |
| integer | Required. Indicates the row number.
Row numbering is 1-based. |
| string1 | Required. The name of the column component, as it is known in the WinStudio form metadata. |
| string2 | Required. A string containing the RGB code value of the color to be used for the background. |
| string3 | Required. A string containing the RGB code value of the color to be used for the foreground. |
The background color is used for the background color of the designated cells. The term "foreground color" typically refers to the font/text color.
The RGB strings consist of a series of three comma-separated integers, each in the range 0–255. For example, the RGB code for a deep purple color might be rendered as (158,44,186).
The use of an empty (null) string ("") tells the system to use the default setting for that value.
Sub Main()
'The following code sets the background color to red
'and resets the foreground color to the current WinStudio default.
ThisForm.Components("grid1").SetGridRowColColorByColumnName(5, "gridColumn1", "255,0,0", "")
End Sub
SetGridRowColFontByColumnName Method
SetGridRowColImageByColumnName Method