WinStudio

SetGridRowColImageByColumnName Method

Applies To

IWSFormComponent interface, grid objects

Definition

Assigns a specified image file to display in a grid cell. This method uses an integer to identify the row number and the column name to identify the column location.

Syntax

object.SetGridRowColImageByColumnName( integer, string1, string2 )

  Part

  Description

object Required. A reference to a grid object.
integer Required. Indicates the row number.

Row numbering is 1-based.

If you use 0 (zero) for this value, the image displays in the header row.

string1 Required. The name of the column component, as it is known in the WinStudio form metadata.
string2 Required. The name of an image file found in the WinStudio executable directory.

NOTE: Supported image file types include *.bmp, *.emf, *.exif, *.gif, *.ico, *.jpg, and *.png.

Remarks

The image file must reside in the same directory as WinStudio.exe.

The height of the cell in which the image appears adjusts automatically to fit the height dimension of the image file. The width of the column can be preset or manually adjusted to accommodate the width of the image.

To clear an image from a particular cell, use this method and pass an empty string (" ") for the image file string.

Example

Sub Main()
   'The following code assigns the graphic file
   'to the third row cell in the column named "CompanyLogo".
   ThisForm.Components("FormCollectionGrid"). _
      SetGridRowColImageByColumnName(3, "CompanyLogo", "MyImage.png")
End Sub

Related Topics

SetGridRowColImage Method

SetGridRowColColor Method

SetGridRowColColorByColumnName Method

SetGridRowColFont Method

SetGridRowColFontByColumnName Method