You must enter a customer record for each of your 
 customers. This record maintains detailed information for the customer 
 and is used throughout the system. The Customers form accesses 
 all the relevant information for storing basic customer data, tracking 
 what customers buy from your company and what they owe you.
	- Open the Customers 
	 form, or the Multi-Site 
	 Customers form if you are working in a master site.
- Turn off Filter-in-Place mode.
- Select Actions > New.
- In the Customer field, do one of these: 
	
		- To define your own customer identifier, enter the alphanumeric 
		 character string to use.
- To allow the system to generate the customer identifier, using 
		 the Customer Prefix defined on the Accounts 
		 Receivable Parameters form, leave the field blank.
 NOTE: The check 
	 mark that is displayed in the top-right corner of the form indicates 
	 that this customer is not on credit hold. If you put this customer 
	 on credit hold, a problem 
	 indicator is displayed on the form. 
- On this form, you can set up a customer record so that a customer 
	 has one Bill To address and multiple Ship To locations: 
	 
	
		- Enter the customer's billing address information in the address 
		 fields.
- To further define the customer's billing information, such 
		 as choosing the customer's language, currency code, and bank information, 
		 enter the appropriate data in the form's fields.
 For more information, see the field descriptions. 
- To save the initial record, select Actions > Save.
- Select the Ship To tab. 
	You can enter up to 9999 different addresses for this customer to 
	 define secondary addresses for shipping purposes: 
		- Click the Ship Tos button located at the bottom of the 
		 tab to open the Customer Ship Tos (or Multi-Site Customer 
		 Ship-Tos)form.
- Select Actions > New.
- In the Ship To field, enter a number or leave the field 
		 blank to accept the next available sequential number. This number 
		 is used on the Customer Order Lines form when you are specifying 
		 a drop-ship-to location.
- On the Address tab, enter the shipping address information 
		 for this ship-to location.
- Select the Codes tab.
- Enter or select appropriate information in the fields. For 
		 more information, see the field descriptions.
- Select Actions > Save to save the ship-to location.
- After you are finished adding ship-to locations, to return 
		 to the Customers form, close the form.
 
- Select the Credit tab. On this tab you can define the amount 
	 of credit extended to the customer. When you add a new customer order, 
	 if that order total exceeds this credit limit, the system displays 
	 a warning message (which you can override). You can also put the customer 
	 on credit hold, which blocks any shipping transactions for this customer. 
	 For more information, see the field descriptions.
- Select the Contacts tab. Specify the names and contact information 
	 for order and billing communications with this customer. For more 
	 information, see the field descriptions.
- Select the Codes tab. Define default codes for this customer. 
	 For more information, see the field descriptions.
- Select the Payment History tab. Enter the initial amounts 
	 for the sales and payment history for this customer. You only need 
	 to do this when you initially set up the customer. The system maintains 
	 most of these values through normal day-to-day transactions. 
	For example, when invoices, debits or credits are posted, the currency 
	 amount of the transaction posts to the Sales PTD field. Invoices 
	 and debits increase the Sales PTD, and credits decrease it. 
	 You update the Average Balance Outstanding, the Largest 
	 Balance Outstanding, and the Last Amount Outstanding values 
	 by running the A/R 
	 Balance History Utility. For more information, see the field descriptions. 
- Select the Corporate Customer tab. This tab allows you to 
	 define a two-tier relationship between separate customer records. 
	 In the Corporate Cust field, if you select this current customer's 
	 customer number, you are specifying this customer as the "corporate 
	 customer." If you select another customer number in this field, 
	 you are specifying this current customer as the "subordinate 
	 customer" (that is, subordinate to the customer you specify in 
	 the Corporate Cust field). 
	Only the customer that you specify as the "corporate customer" 
	 appears on the Bill To tab. This allows you to apply a single 
	 payment across multiple subordinate customer invoices. By selecting 
	 the Corp. Credit field, you can use the corporate customer's 
	 credit values for credit limit processing, or clear this field to 
	 use the subordinate customer's credit values. For more information, see the field descriptions. 
- If European Union codes must be set up for this customer, select 
	 the EUVAT tab and specify the codes. For more information, 
	 see the field descriptions.
- To use revision/pay days for invoicing, select the Revision/Pay 
	 tab. The revision day determines when the invoice is sent to the customers. 
	 The pay day determines when a check can be collected once the invoice 
	 due date is calculated. For more information, see the field descriptions.
- To define sales team/contact information for the customer, select 
	 the CRM tab. For more information, see the field descriptions.
- When you are finished defining this customer record, to save your 
	 changes, select Actions > Save.