Manual Voucher Builder

The Manual Voucher Builder allows you to quickly create a voucher in one or more sites for a single vendor's invoice. On any site, you can specify the portion of the vendor invoice amounts to allocate. You can enter all or some subset of the vendor invoice amounts. You can use the originating site as the To Site.

During processing, the system validates that allocated totals for each type of amount equal the amounts specified from the vendor's invoice. If the validation is successful, the system generates a Builder Voucher number at the Manual Voucher Builder originating site. The Builder Voucher number, along with the Builder Voucher originating site value (the site where Manual Voucher Builder activity is performed) defines the set of vouchers created for this invoice.

The system sets the following values during creation of the voucher at the To Site:

The system sets the following values based upon Terms Code for Vendor at the To Site:

For the A/P Account and A/P Account Unit Codes 1-4, if the Vendor Category exists at the To Site, the system obtains the A/P account and unit codes from the Vendor Category; otherwise, the system obtains them from the Accounts Payable Parameters.

Once the vouchers are created, you may view them on the A/P Vouchers and Adjustments form in the appropriate site.

You can create vouchers outside of the current period under the following conditions:

Data on this form is not persistent. When you close this form, the system removes all non-processed data.

For instructions on using this form, see Creating Vouchers with the Manual Voucher Builder.

You cannot perform the following functions with this form:

NOTE: To perform more complex functions with vouchers, we recommend using the A/P Vouchers and Adjustments form.


Related Topics

Accounts Payable Steps

Creating Multi-Site Vouchers and Adjustments with the Voucher Builder

Creating Vouchers or Adjustments Automatically

Creating Vouchers with the Manual Voucher Builder

Voucher Builder

Vouchers and Adjustments