Accepting Customer Payments in the Euro Currency
If your domestic currency is the euro, or if a customer has converted 
 to the euro, you can accept customer payments in the euro currency.
You can accept payments in the customer's currency, the euro currency, 
 or your domestic currency.
To accept payments in the euro, follow these steps:
	- Set up a bank reconciliation account for the euro currency on the 
	 Bank 
	 Reconciliations form. In the Currency field, enter 
	 the currency code for the euro that you entered on the Currency Codes 
	 form. 
	NOTE: If none 
	 of your customers has converted to the euro currency, this step is 
	 optional. You use this bank account to accept payments from those 
	 customers that use the euro as their domestic currency. 
- When you are ready to process a customer payment (for example, 
	 after you have applied the payment amount to invoices), access the 
	 A/R 
	 Payments form.
- In the Customer field, select the customer ID of the customer 
	 that is making the payment.
- In the Bank Code field, select the code for the bank into 
	 which you are receiving the payment.The bank code must use the same 
	 currency code as either the customer currency or your domestic currency.
- In the Euro Amount field, enter the amount of the payment 
	 in the euro currency. The system converts the amount to the customer's 
	 national currency and to your domestic currency. 
	NOTE: The customer's 
	 balance is reduced by the amount in the Customer Amount field. 
	 The amount in the Domestic Amount field is received into the 
	 specified bank code. The system does not use the amount in the Euro 
	 Amount field; this field simply enables you to enter the euro 
	 payment amount to be converted. 
- Enter any additional data in the remaining fields.
- To save the record, select Actions > Save.
Related Topics
Euro 
 Currency Overview
Setting 
 Up the Euro Currency Code