Authorizing Vouchers
You can control which vouchers to post. However, this
process is optional.
To authorize vouchers:
- On the Purchasing
Parameters form, activate voucher authorization.
For more information, see Activating
Voucher Authorization.
- Create vouchers. For more information, see Creating
Vouchers or Adjustments.
- To select the vouchers to post, run the Voucher
Authorization utility. This utility examines vouchers and
determines whether they can be posted. The default selection processes
all vouchers and adjustments. None of the selection criteria fields
is required, but you can use them to limit the number and type of
vouchers the system processes.
Enter information in these fields, as appropriate:
- Starting and Ending Authorizer
- Enter the range of authorizers. All vouchers authorized by people
whose names fall alphabetically between the starting and ending
names are affected by this utility.
- Starting and Ending Voucher
- Enter the range of vouchers you are authorizing.
- Starting and Ending Invoice Date
- Enter the range of invoice dates for the vouchers you are authorizing.
- Starting and Ending Vendor
- Enter the range of vendors whose vouchers you are authorizing.
- Authorization Status - Enter
the status of the vouchers you are authorizing: F for "failed"
and/or M for "matched."
- Perform one of the following actions:
- To view the results of running the activity or utility without
saving the results in the database, select Preview.
- To save the results in the database, select Commit.
- Select Process.
NOTE: The system
does not post vouchers that have an authorization status of Failed.
- Post the
vouchers you selected in the Voucher Authorization utility.
If Voucher Authorization is not activated, follow your usual
posting procedure to post vouchers.
Related Topics
Accounts Payable
Steps
Posting Vouchers
- Detail
Printing
and Posting Vouchers