Creating Vouchers or Adjustments Manually

You can create a voucher to record an amount you owe to a vendor. You can also create an adjustment to reduce the amount of a previously entered voucher.

NOTE: You can also create vouchers or adjustments automatically. After you receive the purchase order, use the Generate A/P Transactions utility to create the vouchers or adjustments, or configure your vendors to allow generation of vouchers immediately after receiving a shipment by using the Auto Voucher field.

To print a new voucher with adjusted amounts, you must first negate the original voucher entirely. Using the PO Receiving form, perform a debit return for the same quantity originally vouchered. The system generates an adjustment to offset the corresponding voucher, allowing you to begin again. Then, receive the quantity back in. The new voucher can now be generated with the corrected domestic currency amount.

  1. Open the A/P Vouchers and Adjustments form.
  2. Select Actions > New.
  3. In the Vendor field, select the vendor for which you are entering the voucher or adjustment.
  4. Specify information in these fields:
  5. Under the Tax and Authorization tab, enter data in the following fields:
  6. Select the Amounts tab, and specify information in these fields:
  7. Select Actions > Save.

Related Topics

Accounts Payable Steps

Creating Multi-Site Vouchers and Adjustments with the Voucher Builder

Posting Vouchers - Detail