Creating Vouchers with the Manual Voucher Builder

The Manual Voucher Builder form allows you to quickly create a voucher in one or more sites for a single vendor's invoice. On any site, you can specify the portion of the vendor invoice amounts to allocate. You can enter all or some subset of the vendor invoice amounts. You may use the originating site as the To Site.

  1. Set up Replication Rules for the Voucher Builder category. This is a one-time setup.
  2. Open the Manual Voucher Builder form.
  3. Enter the following information in the header:
  4. In the grid for each site, enter the following information. Allocation totals display at the bottom of the form.
  5. To generate the vouchers for each site, click Process.

    If validation is successful, the system creates the pending voucher transactions in the site(s) specified. It generates a new Builder Voucher number based on the originating sites Purchasing Parameters and the last Builder Voucher number. The Builder Voucher Orig Site is set as the site specified on the the General Parameters form where you are creating the manual voucher.

    If validation fails, the system handles the failure in one of the following ways:

The new Builder Voucher number is displayed in a message when processing is complete.

When you close the form, the system removes any unprocessed rows.


Related Topics

Creating Multi-Site Vouchers and Adjustments with the Voucher Builder

Creating Vouchers or Adjustments Manually

Reversing a Voucher Generated from Purchasing