Running APS Planning
To run the APS plan, use the following procedure. 
 This procedure deletes the existing plan and recreates it using the latest 
 demand and capacity information.
	- Make sure the planner database is running.
- Navigate to the APS 
	 Planning form. 
	NOTE: Run this 
	 activity only at times when no other users will be saving changes 
	 to records that are included in the plan. You can run it on a recurring 
	 basis by scheduling it on the Background Queue. For more information, 
	 see Scheduling 
	 Reports and Utilities to Run in the Background. 
- Select whether to generate the plan for this local site (Single-Site 
	 Plan) or for all sites (Global Plan).
	
		- A global plan generates transfer orders for any remote components 
		 using up-to-date planning data at the remote site. To use this 
		 option, multiple sites must be defined using the Sites/Entities 
		 form. Those sites must also be defined on the APS 
		 Sites and Alternative Management form. The site you 
		 are logged in to must be configured as the "local" site 
		 on the APS Sites and Alternative 
		 Management form and the other sites must be configured 
		 as "remote" sites.
- A single-site plan can generate transfer orders, but the system 
		 generates them using the item lead time and transit time (you 
		 can replicate them to the supply sites using the planning replication 
		 category).
 
- To start the APS planning activity, click Plan.
	The system displays the message: Task Submitted. 
- To find out if the process completed successfully, open the Background 
	 Task History form.
	If the planning task appears in the list with a Return Status 
	 of 0 (Complete), the task completed successfully. 
- When the process is finished, you can view the new planned orders 
	 and exception 
	 messages using the Planning Detail 
	 form or the Material Planner Workbench.
- You can also analyze 
	 the plan output using one of several output analysis forms to 
	 determine bottlenecks in your resource capacity and to determine how 
	 your supplies are being used.
If any errors occur during this process, view the ERRORLOG table in 
 the SyteLine 
 SQL database for a more detailed error message. For more information, 
 see Troubleshooting 
 APS.
Related Topics
APS Overview
APS Planning
About 
 Global Planning
Analyzing 
 APS Output
Planning Parameters
Refreshing 
 the APS Plan to Reflect Changes