Using Project Advance Payments
This help topic discusses how advance payments relate to projects. For
general information about projects and project tasks, use the links below
or the menu bar.
Project Settings
- On the Project
Parameters form, define the general ledger account that will be
used to record invoices generated from an advance
payment invoice. If advance payment is received before an invoice
is sent to the customer, the money is recorded as an open payment.
After an advance payment invoice is generated, the money is moved
to the advance payment account.
- Create
a project with a WIP
Relief Method of Revenue Recognition.
Revenue Milestones
- Open the Revenue
Milestones form and create a milestone for the project you just
created. Select the Create Advance Payment Invoice field.
Nominate the revenue milestone on the Revenue
Milestone Nomination form.
NOTE: If you
attempt to nominate a milestone that will cause the total advance
payment deduction amount to exceed the total amount invoiced, an error
displays and the milestone is not nominated.
- Post the revenue milestone on the Print/Post
Project Revenue Milestones form. This action causes an invoice
milestone to be created with the same settings as the revenue milestone.
After posting the revenue milestone, the Projects form is updated
with the advance payment information defined on the milestone.
Invoice Milestones
- Create the advance payment on the Invoice
Milestones form if one was not automatically generated from a
revenue milestone. Enter the invoice information, then select the
Create Advance Payment Invoice field.
Nominate the invoice milestone on the Invoice
Milestone Nomination form.
NOTE: If you
attempt to nominate a milestone that will cause the total advance
payment deduction amount to exceed the total amount invoiced, an error
displays and the milestone is not nominated.
Invoicing and Additional Milestones
- Create A/R invoices on the Post
Project Invoice Milestones form. If an A/R invoice is generated
for a milestone marked as an advance payment invoice, the distribution
uses the general ledger advance payment account defined on the Project
Parameters form.
- If an A/R invoice is generated for a milestone marked as an
advance payment, the distribution should use the general ledger
advance payment account defined on the Project
Parameters form.
- If an A/R invoice is generated for a milestone not marked
as an advance payment, the invoice will be reduced by amount entered
in the Advance
Payment Deduction Amount field, and will use the Unbilled
A/R account.
- When payment is received, post the advance payment transaction
on the Invoice
Posting form.
- As new milestones are created, use the Advance
Payment Deduction Amount field to define how much of the advance
payment to apply to each invoice. When entering an amount in the Advance
Payment Deduction Amount field, the To be Deducted field on the
Projects
form is updated when you save the milestone.
- Check the Projects
form for a summary of advance payment balances and invoice deductions.
Related Topics
Projects Overview
Accounts
Receivable Steps
Create A Project
Create a
Project Resource
Create a Project
Task
Create a
Revenue Milestone