Shop-Trak Label Permission Hierarchy & Options

Shop-Trak looks for label permissions and options in the following order:

Shop-Trak Parameters - Main Tab

Shop-Trak first verifies that the Labels check box is selected on the Main tab of the Shop-Trak Parameters form.  When this check box is enabled, the Labels option displays on the Shop-Trak Shop Floor menu and allows employees to print labels.

Shop-Trak Parameters - Labels Tab

Next, Shop-Trak checks the Label Parameters to see what types of Labels are allowed to print on the shop floor: (O)peration to Operation, Operation to (S)tock, or neither.  If no options are entered, no labels will print.  If either (O), (S), or both are entered, Shop-Trak will then check the Employee Profile.

NOTE:  If Kanban or Bin is selected, then the option to print these labels will appear on the Info tab.  

Employee Profile - General Tab

Shop-Trak then checks the General tab of the Employee Profile.  If the Use Main Parameters check box is selected for the employee, Shop-Trak will verify that the Labels check box is selected in the Available Menu Options section.  If it is not, no labels will print.

If the Use Main Parameters check box is not selected, and the Labels check box is not selected, the employee will be allowed to print labels depending on the types allowed in the Label Print Options section on the Labels tab of the Shop-Trak Parameters form.  The ability to print Labels on the shop floor may be granted or revoked via the Employee Profile.

Note:  Label printing defaults to Off’ upon the installation of Shop-Trak.

 


Related Topics

Shop-Trak Defining Label Rules

Shop-Trak Customizing Default Labels

Shop-Trak Tables & Fields for Custom Labels

Shop-Trak Creating & Printing Employee Badges

Shop-Trak Defining Labels Parameters

Shop-Trak Setting Up the Employee Profile - General Tab