This topic summarizes how the Shop-Trak Label Rules form is used to create rules for labels and also shows label rule examples.
There are six default labels located in the BTLabels folder on your Shop-Trak CD or download location:
The labels can be used as-is, or modified to suit you organization's needs.
Labels can also be printed for JIT Transactions. Simply add a label rule specific for the JIT Item. The label rule would use the type O for Operation to Stock. When completing pieces and moving them to stock, the label for that item will be called and printed to the printer specified in the Label Rule.
Rules for Kanban and Bin labels can be defined by specifying the workstation Login Name field. Rules for Operation to Operation, Operation to Stock, and Material to Stock labels can be defined by specifying the following fields:
| Type | S |
| Item | * |
| WC | * |
| Product Code | * |
| Cust Num | 100 |
| Login Name | * |
| Label Name | Customer100stock.btw |
| Printer | \\servername\PrinterA |
Result - When pieces are completed on the last operation of a job for Customer 100, Shop-Trak will find the label format called Customer100stock.btw in the format path specified in the Label Parameters and send it to PrinterA.
| Type | S |
| Item | FG-1000 |
| WC | * |
| Product Code | * |
| Cust Num | 100 |
| Login Name | * |
| Label Name | Customer100stock.btw |
| Printer | \\servername\PrinterB |
Result - When pieces are completed on the last operation of a job for Customer 100 and the item is FG-10000, Shop-Trak will find the label format called Customer100stock.btw in the format path specified in the Label Parameters and send it to PrinterB.
| Type | O |
| Item | * |
| WC | AS-500 |
| Product Code | * |
| Cust Num | 200 |
| Login Name | * |
| Label Name | Customer200move.btw |
| Printer | \\servername\PrinterA |
Result - When pieces are completed at WC AS-500 on a job for Customer 200, Shop-Trak will find the label format called Customer200move.btw in the format path specified in the Label Parameters and send it to PrinterA.
| Type | M |
| Item | CP-10000 |
| WC | * |
| Product Code | * |
| Cust Num | * |
| Login Name | * |
| Label Name | ReturnToStock_CP-10000.btw |
| Printer | \\servername\PrinterB |
Result - When a Job Material Withdrawal Transaction is performed for item CP-10000, Shop-Trak will find the label format called ReturnToStock_CP-10000.btw in the format path specified in the Label Parameters and send it to PrinterB.
| Type | K |
| Login Name | Stockroom |
| Label Name | kanban.btw |
| Printer | \\servername\PrinterA |
Result - When Stockroom is logged on to this workstation on the shop floor, Kanban labels will print to PrinterA. Multiple rules can be setup for individual logins. The printer will default to the printer defined in the rule above, or the user can choose from a list of printers available to that workstation. Bin labels are handled the same as Kanban labels.
Shop-Trak Defining Labels Parameters
Shop-Trak Customizing Default Labels
Shop-Trak Label Permission Hierarchy & Options
Shop-Trak Tables & Fields for Custom Labels
Shop-Trak Label Permission Hierarchy & Options
Shop-Trak Creating & Printing Employee Badges
Shop-Trak Setting Up the Item Profile for Kanban Replenishment