Shop-Trak Setting Up the Employee Profile - General Tab

Use the General tab of the Shop-Trak Employee Profile form to add or change an employee ID, print an employee badge, and define employee menu options for Shop-Trak Shop Floor.  These settings will override those on the Main tab of the Shop-Trak Parameters form.

To set up General options for an employee:

  1. Open the Shop-Trak Employee Profile form.
  2. Click the General tab.
  3. Specify this information:

Shop-Menu Options

Use Main Parameter Defaults

Select this check box to set the employee’s Shop-Trak Shop Floor menu options to those defined in the Available Menu Options section on the Main tab of the Shop-Trak Parameters form.  The menu options on the Parameters Main tab are used to define the company standard.  Employees outside of the company standard would have menu options defined uniquely on the Shop-Trak Employee Profile form.

Available Menu Options

Specify which transaction types and option buttons the employee will see in Shop-Trak Shop Floor.  Most combinations of these options are valid.  These settings will override those specified on the Shop-Trak Parameters form.  See the Available Menu Options section of the Shop-Trak Defining Main Parameters topic for definitions of options, except for the following which reside only on the Shop-Trak Employe Profile form:

 


Related Topics

Shop-Trak Employee Profile Form

Shop-Trak Defining Main Parameters

Shop-Trak Setting Up an Employee to Perform Backflushing of Lots & Serials

Shop-Trak Creating & Printing Employee Badges

Shop-Trak Break Lunch Schedule and Methods