Shop-Trak Setting Up an Employee to Perform Backflushing
of Lots & Serials
This topic describes how to set up an employee to perform backflushing
of lot and serial tracked materials from Shop-Trak Shop Floor.
Specify the information described below on the
Inventory Parameters, Items,
Shop-Trak Employee Profile, and Shop-Trak Work Center Profile forms.
Inventory Parameters Form
- Open the Inventory Parameters
form.
- On the General tab, select
the On Hand Neg
Flag check box.
- On the Control tab, select
one of the following, or both:
- Backflush
Lot Numbers check box
- Backflush
Serial Numbers check box
- Save changes and close the form.
Items Form
- Open the Items form.
- Click the Controls tab.
- Select the Backflush
check box.
- The Backflush Location can be selected here but is not
required. The standard Infor SyteLine Backflushing
Hierarchy is used to find the backflush
location. For more information, please refer to the About Backflushing
Materials topic in the Infor
SyteLine Online Help.
NOTE:
Backflushing will only use inventory
from the Default Warehouse identified on the Control
tab of the Inventory Parameters
form.
- Save changes and close the form.
Shop-Trak Employee Profile Form
- Open the Shop-Trak Employee
Profile form.
- Click the General tab.
- Select the Backflush
Lots/SNs check box to display the
Backflush
Lot & Serial button on the Materials
tab in Shop-Trak Shop Floor. Clicking
this button will display the Select
Backflushed
Lots and Serial Numbers form in Shop-Trak
Shop Floor. The employee can then access this form if the requirements
for the lots and serials were not fulfilled at the time the transaction
was ended. Transactions will remain in this form until the lot
or serial fulfillment is complete.
- If you want to allow the employee to perform backflushing
for transactions created by any
employee, click the Controls
tab and select the Backflush
Administrator check box.
Clearing this check box allows the employee to perform
backflushing only on transactions
they create.
- Save changes and close the form.
Shop-Trak Work Center Profile Form
- Open the Shop-Trak Work
Center Profile form.
- Add a new record for the work center where the backflushing
will be performed.
NOTE: This
is the work center where the completed pieces are being reported. This
may or may not be the work center of the operations where the backflushed
materials exist.
- Click the Controls tab.
- In the Backflush
Required field (applies to Run, Setup, and WIP Move transactions only), specify when
the assigning of lots or serials can be performed: N (Never),
P (Prompt), or R
(Required).
- N (Never) - Select
N to never prompt the
employee to select lots and serials when entering or completing
a transaction in this work center. The
transaction is sent to the Select Backflushed Lots and Serial Numbers form in Shop-Trak
Shop Floor. Transactions remain in this form until the lot
or serial number fulfillment is complete. The backflushing requirements are performed
at a later time. This is the default setting for any
pre-existing work center profiles.
NOTE: Due to the method Shop-Trak uses to split quantities complete to
each team member, Team work centers always default to
N (Never). Team transactions
always go to the Select Backflushed Lots and Serial Numbers form in Shop-Trak
Shop Floor for lot and serial assignment. The Team Leader
will not be allowed to select the
lots and serials at the time the Team transaction is ended.
- P
(Prompt) - Select P
to prompt the employee by displaying the Backflushed Lot
and Serial Number Selection form. Partial or
full completion of the backflushing
requirements can be performed. The employee can also choose
to send the transaction through without selecting any lots or
serials. If the full backflushing
requirements have not been met, the transaction is saved to the Select Backflushed
Lots and Serial Numbers form for the backflushing to be performed at a later
time by a Supervisor or Backflush Administrator.
- R
(Required) - Select R
to require the employee to
fulfill all the lot and serial number assignments prior to completing
the transaction. The employee is not allowed to leave
the form until all backflushed
materials' lots and serials are selected. If there are not
enough lots or serial numbers available in inventory, the employee
is not able to end the transaction until the quantities available
in inventory are adequate to fulfill the backflushing
needs. The employee will need to address the situation
with a Supervisor and correct the inventory condition in Infor SyteLine in
order to proceed. Transactions that have all the lots or
serials assigned at the time the employee ends the transaction
will then transfer and post to Infor
SyteLine.
- Save changes and close the form.
Related Topics
Shop-Trak
Backflushing of Lots & Serials
Overview
Shop-Trak
Setting Up the Employee Profile - General Tab
Shop-Trak
Work Center Profile
Shop-Trak
Editing Transactions
Shop-Trak
Reviewing Pending Inventory & Material Transactions