Shop-Trak Approving & Adjusting Transactions
When setting up the Options
tab of the Shop-Trak Employee Profile,
the Administrator can require that employee transactions be approved by
a Supervisor before the transactions are transferred to Infor SyteLine.
The Supervisor will then use the Shop-Trak
Approval and Adjustments form to display the employee transactions
for review and approval. The Supervisor can also use this form to
make minor adjustments to posted
transactions.
Setting
Up Supervisory Approval
Form Buttons
Retrieving
Records for Approval & Adjustment
Summary Tab
Detail Tab
Adjusting Hours
Approving Hours
Operational Tab
These steps are performed by the Administrator.
- On the Options tab of the
Shop-Trak Employee Profile
form, specify the Primary,
Alternate (optional),
and Admin
(optional) Supervisors.
- Select the Require Transaction
Approval check box. Checking this option requires the
employee's transactions to be approved before allowing the transactions
to transfer to SyteLine. However this option does not
need to be checked in order for a Supervisor to adjust transaction
hours.
You can access additional forms throughout the approval and adjustment
process using the following buttons:
- Shop-Trak Edit List Report
- Opens the Shop-Trak Edit List Report and populates the employee
number along with starting and ending work dates.
- Shop-Trak Employee Profile
- Opens the Shop-Trak Employee Profile form for the selected employee.
- Shop-Trak Edit Transactions
- Opens the Shop-Trak Edit Transactions form and displays the employee's
transactions for the selected date. If the transaction
is already posted this button will not be available.
- Unposted Transactions -
Opens the Unposted Transactions form and displays the employee's transaction
for the selected date. If you created an adjusting transaction
in error or that needs to be removed, you will need to go the Unposted
Transaction form to remove it. If there are no transactions
for the selected date, this button will not be available.
- Project Labor Transactions
- Opens the Project Labor Transactions
form. This button is available if the transaction is still in
the Project Transactions form.
The steps in this section and the remaining sections are performed by
the employee's Supervisor.
- Open the Shop-Trak Approval and
Adjustments form.
NOTE:
While the Shop-Trak Approval and Adjustments form is open, the
employee is not locked. This is by design as this form could
be open for some time as data is reviewed.
- Unfilter to view all records
for employees you supervise, or filter for specific records using
the following fields:
- Employee - Employee
number from Employees
form.
- Primary or Alternate Supervisor
- The employee's primary and alternate supervisors.
- Week Ending or
Reporting Date
- Reporting Date - Groups
all transactions for the same work date together using the
Reporting + Payroll Date
from the Shop-Trak Break
Lunch Schedule form. Viewing by Reporting Date
is useful for shifts that cross midnight.
- Week Ending - Groups
a seven day range of transactions together based on the date
selected. Viewing by Week Ending date is useful for
approving a complete week at a glance.
- Select a date from the calendar. If you selected
Reporting Date above, select the End
of Shift or Start
of Shift date. If you selected Week Ending, the
date you select will include transactions from the seven
days prior to and including that date.
- Shift - Employee's
default shift number.
- Shop-Trak looks for the employee transaction records meeting
the criteria specified. It also looks to see if those transactions
have been approved or not. If all transactions have been approved,
it notifies you with the message "There are no records to approve."
However, you can still create adjusting transactions to posted transactions.
- Records meeting the criteria are returned in the grid view.
To view an employee record on the Summary
tab:
- Select an employee record in the grid view.
- The employee record then displays on the Summary
tab.
- The Total Hours field at
the top of the form will display the total hours for the day. The Hrs to Approve
field at the top of the form will display the hours that have yet
to be approved. The
Summary tab will show Approved
hours and Not Approved hours
in separate columns.
Use this tab to view all transactions for the employee record selected.
Only the transactions that have been posted can be adjusted. The
posted transactions will have a check mark in the Posted
column. Work Center transactions
cannot be adjusted. You will need to manually create either a positive
or negative transaction in the Shop-Trak
Edit Transactions form.
Both payroll and manufacturing hours are adjusted. You cannot
adjust a transaction if there are no payroll hours. For example,
in a set of transactions such as Start Additional (split by rate), only
the transaction containing the payroll hours can be adjusted.
IMPORTANT:
In order to make adjustments, you must
be designated as a Supervisor on the Shop-Trak
Employee Profile form. However, the Require
Transaction Approval check box does not
need to be selected in order to make adjustments.
To adjust employee hours:
- Arrange the columns to your personal preference.
- Enter the amount of the adjustment in the Adjust
column. Use positive numbers to add time and negative numbers to
subtract time. Enter the time in decimal format (you can enter
up to the third decimal level). For example, if the transaction
hours are 4.25 and you want to change them to 4, you would enter -.25.
If you wanted to change the hours to 5, you would enter .75.
- If you enter an amount into the Adjust
field that is greater than the time in the
Pay Hours field, a message displays stating "Adjust Hours
is greater than Payroll Hours." Click OK.
A message displays asking "Do you want to change now?"
Click Yes to revise
the adjustment. Click No
to leave the adjustment in the field. However you will not be
able to save until the adjustment is removed or corrected.
- If the Job Status or Job Operation Status are complete,
a message displays stating "Job is Closed or Operation is Complete.
Please enter in an Indirect Code." Press OK.
Select an Indirect Code
from the Ind
Code column and a new transaction will be created for the selected
code.
- Click Save.
- The adjusting transaction is created and displays in the top row.
Additional adjustments to the same or other transactions display
in the row beneath the most recent adjustment. The original
transaction is not changed.
- The Total Hours column
will reflect the revised total for all transactions, including
the adjustments.
- Both the Pay Hours (payroll)
and Mfg
Hours (manufacturing) are
adjusted. For a Start Additional set of transactions, only the
transaction with the payroll hours will be adjusted. If there
are no payroll hours, a message will display stating that only the
manufacturing hours will be adjusted.
- After adjustments are made:
- The message "Added Manually"
will appear on the Shop-Trak
Time & Attendance / Delinquency Report
for the adjusted transactions.
- The adjusting
transaction will:
- Remain in the Unposted
Job Transactions form until manually posted or until
the Shop-Trak Background Polling process runs.
- Include the initials of the Supervisor that created it.
NOTE: The Supervisor
must have their initials entered into the Additional
Info tab of the Users form.
- Not include any start or end times.
To review and approve individual transactions:
- Select the Approved
check box for that transaction. Only completed transactions
(transactions with start and end times) can be approved.
- To select all transactions for approval, click Approve
All.
- To deselect all transactions checked for approval, click Unapprove
All.
- Once approved, transactions
will transfer automatically via the Shop-Trak Background Polling process,
or manually using the Shop-Trak
Transfer Transactions to SyteLine form.
- The
Trx Close Job and Trx Oper Complete fields will be checked if
the employee closed the job/operation during the transaction. To update
this field, click the Shop-Trak
Edit Transactions or Unposted
Transactions buttons.
NOTE: Daily transactions that have already
been approved and transferred will continue to display on the Shop-Trak
Approval & Adjustments form. This gives the Supervisor the ability
to see the complete set of transactions for the day.
Use this tab to view calculations and additional information about the
transaction selected on the Detail
tab. This tab is read-only. You can arrange the columns to
your personal preference.
- Reference - Code made up
of transaction type or indirect code, job-suffix operation, and project
number.
- Trx
Qty Complete - Quantity complete
on this transaction.
- Trx
Qty Moved - Quantity moved on this
transaction.
- Trx
Qty Scrapped - Quantity scrapped
on this transaction.
- Scrap reason code - Scrap
reason selected for this transaction.
- Qty
Worked On - Quantity worked on for a multi-job transaction.
- Std
Hrs/Piece - Job operation labor hours
per piece.
- Std
Pieces/Hr - Job operation pieces per
labor hours.
- Trx
Hours - Actual hours on this transaction.
- Efficiency Ratio(%) - Calculation
= Standard plan/earned hours / actual job hours.
- WC - Work center for the
operation on this transaction.
- Item - Job item.
- Description - Item description.
- Job Status - Job status.
- Job Oper
Status - Job operation status.
- Qty
Released - Job released quantity.
- Qty
Posted - Operation posted quantity.
- Qty
Unposted - Operation quantity complete in Shop-Trak Edit Transactions
or Unposted Transactions forms.
- Trx Close Job - Indicates
whether or not the job was marked complete with this transaction.
- Trx Oper Complete - Indicates
whether or not the operation was marked complete with this transaction.
- Whse - Warehouse name.
- Last Oper of Job - Indicates
whether or not this was the last operation of the job.
- Scrap Percentage - Calculation
= Transaction quantity scrapped / (transaction quantity complete +
transaction quantity scrapped) * 100.
- Mfg Cost - Calculation
= Transaction hours * job cost rate on the transaction.
- Remaining Run Hours - Calculation
= (Job quantity released - jobroute.qty_complete)
* run labor or run machine hours.
- Control Point - Indicates
whether or not the operation is the control point.
- Sched Driver - Operation
schedule driver from the job route.
- Use Fixed Schedule - Indicates
whether or not the operation uses fixed schedule hours.
- Fixed Sched Hours - Operation
fixed schedule hours.
- Trans Type - Transaction
type.
- Job - Transaction job number.
- Sufffix - Transaction suffix
number.
- Oper Num - Transaction
operation number.
- Project Number - Transaction
project number.
- Task Number - Transaction
project task number.
- Cost Code - Transaction
project cost code.
- Ind code - Transaction
indirect code.
- Source - Name of the database
table where the transaction resides.
Related Topics
Shop-Trak Approval
& Adjustment Form
Shop-Trak Setting
Up the Employee Profile - Options Tab
Shop-Trak Editing Transactions
Shop-Trak Reports
Listing