WinStudio
IWSIDOCollection interface
Sets the value of a specified property of the current object in an IDO collection.
object.SetCurrentObjectProperty( string1, string2 )
Part |
Description |
| object | Required. A reference to a valid IDO collection object. |
| string1 | Required. The name of the current object property. |
| string2 | Required. The value of the current object property. |
This method does not mark the property as "modified" or notify dependents (such as components bound to the property) to refresh.
This is particularly applicable to date/time values. Localized date values can be displayed, for example, as dd/mm/yyyy, mm/dd/yyyy, or mm/dd/yy. When such a value is used, the system tries to interpret the appropriate display value for the property. A system internal value, however, uses the format yyyy/mm/dd, and it never changes. So, to use the internal value, your input value must conform to this format.
NotifyDependentsToRefresh Method
SetCurrentObjectPropertyModified Method
SetCurrentObjectPropertyPlusModifyRefresh Method
SetObjectPropertyModified Method
SetObjectPropertyPlusModifyRefresh Method