WinStudio
IWSIDOCollection interface
Sets the value for a property of the current object, marks the property modified, marks the object modified, and notifies any dependents, such as components bound to the property, to refresh.
object.SetCurrentObjectPropertyPlusModifyRefresh( string1, string2 )
Part |
Description |
| object | Required. A reference to a valid IDO collection object. |
| string1 | Required. The name of a property of the current object. |
| string2 | Required. The value of the property named by string1. |
For information about other methods and properties that you can use to set the value of a property or perform one or more of the other operations performed by this method, see the Related Topics.
This method is equivalent to executing the following four low-level methods:
This is particularly applicable to date/time values. Localized date values can be displayed, for example, as dd/mm/yyyy, mm/dd/yyyy, or mm/dd/yy. When such a value is used, the system tries to interpret the appropriate display value for the property. A system internal value, however, uses the format yyyy/mm/dd, and it never changes. So, to use the internal value, your input value must conform to this format.
NotifyDependentsToRefresh Method
SetCurrentObjectProperty Method
SetCurrentObjectPropertyModified Method
SetObjectPropertyModified Method
SetObjectPropertyPlusModifyRefresh Method