WinStudio
IWSIDOCollection interface
Sets the value for a property of an object, marks the property as "modified", marks the object as "modified", and notifies any dependents, such as components bound to the property, to refresh.
object.SetObjectPropertyPlusModifyRefresh( string1, long, string2 )
Part |
Description |
| object | Required. A reference to a valid IDO collection object. |
| string1 | Required. The name of a property of an object. |
| long | Required. A long integer that specifies the row
number of the object.
The number of the first row in a collection is 0. |
| string2 | Required. The value of the property. |
For information about other methods and properties that you can use to set the value of a property or perform one or more of the other operations performed by this method, see the related topics.
This method is equivalent to executing the following four methods:
Sub Main()
If ThisForm.Variables("EnteredValue").Value <> _
ThisForm.PrimaryIDOCollection.GetObjectProperty("TaskDescription", 1) Then
ThisForm.PrimaryIDOCollection.SetObjectPropertyPlusModifyRefresh _
("TaskDescription", 1, ThisForm.Variables("EnteredValue").Value)
End If
End Sub
NotifyDependentsToRefresh Method
SetCurrentObjectProperty Method
SetCurrentObjectPropertyModified Method
SetCurrentObjectPropertyPlusModifyRefresh Method
SetObjectPropertyModified Method