Generating Vouchers
Vouchers can be generated:
When you generate vouchers, remember this information:
- Before any transactions are created, the total distributed cost
of the PO must equal the sum of all vouchered line/releases. If they
are not equal, the system displays an error message.
- If you are creating an adjustment rather than a voucher, you must
select the number of the voucher you are adjusting.
- When generating an adjustment, the A/P transaction record is filled
with values from the A/P posted transaction record. The transaction
type is A, and the reference begins with APA.
- As each line/release is processed, the Unit Cost field of
the purchase order is set to the vouchered unit cost, and the purchase
order detail costs are set to the vouchered detail costs.
- While transactions and distributions are set, messages display
if the corresponding account number has not been set up on the Accounts
Payable Parameters form (the message is only a warning, and processing
continues).
- If the cost method is Actual or Standard, the system
displays a message if the corresponding account numbers are not set
for the line item.
- The following A/P distribution transaction records are created
when you generate vouchers:
- The PO line/release quantity vouchered is set to the quantity received
minus the quantity returned.
- The PO line/release quantity returned is set to zero.
When all transactions and distributions are created, the system displays
a message indicating that the process is complete.
Related Topics
Creating
Multi-Site Vouchers and Adjustments with the Voucher Builder
Creating
Vouchers or Adjustments Automatically
Creating
Vouchers or Adjustments Manually