To print and post payroll checks:
The system updates the upper grid with a list of the current payroll transactions to be processed, based on the selected printing options. The current payroll transactions are validated for correct G/L accounts and balanced distributions. If the distributions are not in balance, you should print the Payroll Distribution Log Report to determine the cause of the imbalance.
When the transactions are in balance, you can print the payroll checks.
TIP: If necessary to void checks, select the Void Check(s) option and then click Process. For more information, see the Voiding Checks in a Pay Period, Voiding Posted Payroll Checks, and Voiding a Posted Check Manually Help topics.
When you post payroll, the following updates occur: