Costing Setup
We strongly recommend you decide on a coherent, overall
costing strategy for your company before implementing any of the costing
functionality in the system.
Be sure you understand the implications of the cost type and cost method
you have chosen before you implement the manufacturing functions. After
your strategy is complete, you can set up the system to handle the associated
calculations and controls and provide the appropriate cost reports. You
implement your strategy by indicating your decisions on the following
fields, which control the way the system maintains, processes, and applies
costs throughout the system:
| Form |
Field |
| Inventory Parameters |
Cost Type |
| Cost Item at Warehouse |
| General Parameters |
Post to Journals |
| Purchasing Parameters |
Update Current Cost |
| Shop Floor Control Parameters |
Calculate Variances Against |
| Overhead Basis (Material, Labor, Machine) |
| Cost Based on Complete (Operations, Jobs) |
| Items |
Cost Type |
| Cost Method |
- Open the Inventory
Parameters form and select a cost type in the Cost Type
field. The cost type you select at this level will be the default
value in the Cost Type field when you add new item records. On the
Items form - General tab, you can overwrite the Cost Type on
an item by item basis. Valid options are:
Standard Costing:
- All inventory reports use the standard cost of each item.
- All transactions processed that affect inventory value are
posted to the inventory distribution journal at standard cost
(variances are also posted).
- You can still use one of the four actual cost methods (average,
LIFO, FIFO, or specific) for job costing, even though you are
using standard costing for your journals/ledger.
- Variance calculation will depend on the setting of the Calculate
Variances Against field located on the Shop Floor Control Parameters
form. For standard costing, this field should be set to Standard.
Actual Costing:
- All inventory transactions are posted to the inventory distribution
journal based on the cost method you enter for each item on the
Items form.
- The cost used for inventory reports, job costing, and posting
to the inventory ledger distribution journal is determined by
the costing method specified in Items for each item.
- Variance calculation will depend on the setting of the Calculate
Variances Against field located in Shop Floor Control Parameters.
For actual costing, this field should be set to Actual.
- Select the Cost
item at Warehouse field if you want to track the cost of items
at the item/warehouse level instead of the item level. Leave this
field blank to continue to track costs at the item level.
CAUTION: Once you select this
field and save the record, it cannot be deselected.
- Open the General
Parameters form and select the Post to Journal check box
if you want the system to post to the Ledger Distribution Journals
transactions for all production and material transactions. Clear this
check box if you do not want the system to perform the posting.
- Open the Purchasing
Parameters form and select a value in the Update Current Cost
field. This field tells the system how to use the Current Unit Cost
field in Items for purchased items. Regardless of which costing
method is in use, it is possible to use the Current Unit Cost field
to maintain the current cost of purchased parts. The value of this
field has no affect on the flow of costs through the system. It is
accessed only by the purchase order receiving function in Purchasing
to determine whether it is possible to update the Current Unit Cost
field in Items with the purchase price of the item. The valid
values for this field are:
- Average - The system maintains
the average purchase cost for purchased items in the Current Unit
Cost field. When an item is received into stock by way of the
purchase order receiving function, The system calculates a new
average cost for the item and posts the result back to the Current
Unit Cost field.
- Last - The system maintains
the last price paid for purchased items in the Current Unit Cost
field. When an item is received into stock through the Purchasing
module, the purchase order unit cost is posted to the Current
Unit Cost field.
- None - prevents Purchasing
from updating the Current Unit Cost field when items are received.
- Specify information on the Shop
Floor Control Parameters form:
- Jobs Tab - Calculate Variances
Against - Select Actual or Standard.
Transactions Tab - Overhead
Basis determines whether the overhead costs applied to jobs
are based on material cost, labor hours, both, or neither. Enter
the Overhead Applied Basis. If you leave this field blank, the
system will not calculate overhead. Valid entries are:
- Labor - the Fix Ovhd
Rate and Var Ovhd Rate fields on the Departments form
are used in the calculation of labor overhead.
- Material - the Fixed
Matl Ovhd Rate and Variable Matl Ovhd Rate tabs on the Product
Codes form are used in the calculation of material overhead.
The overhead updates the WIP when you issue the material to
the job.
- Machine - the Fix Mach
Ovhd Rate and Var Mach Ovhd Rate fields on the Work Centers
form-Costing tab are used in the calculation of machine overhead.
- Transactions Tab - Costs Based
on Complete determines how costs are calculated for items
moved to stock from non-completed jobs. Valid entries are:
- Operations - actual costs
are used for those operations that are complete; planned costs
are used for those that are incomplete.
- Jobs - planned costs
are used for all operations.
- Specify information on the Items
form:
- Cost Type - displays the
cost type you entered as a default on the General Parameters form.
If you want to overwrite the default for the current item only,
select Actual costing or Standard costing. When you change the
Cost Type, the system converts the internal information to match
the new type for the item. This may generate ledger transactions.
- Cost Method - maintains the
cost flow method used for tracking and posting Cost Ledger transactions
for the item. When you change the cost method, the system will
convert the internal information to match the new method for the
item. This may generate ledger transactions.
NOTE: When determining
the values it should use for posting to the journals/ledger, the system
first looks at the Cost Type in Items. If the Cost Type is Standard,
the system will post the standard unit costs for all items to the journals/ledger.
But if the Cost Type is Actual, the system will look at the Cost Method
to determine the values it should post to the journals/ledger.
The cost flow methods available for valuing inventory if your Cost Type
is set to Actual are:
| Cost Type |
Cost Method |
| Actual |
Average |
| Actual |
LIFO |
| Actual |
FIFO |
| Actual |
Specific |
The cost flow methods available for valuing inventory if your Cost Type
is set to Standard are:
| Cost Type |
Cost Method |
| Standard |
Average |
| Standard |
LIFO |
| Standard |
FIFO |
| Standard |
Specific |
| Standard |
Standard |
Related Topics
Costing Overview
Average Costing
Setup
LIFO and
FIFO Costing Setup
Specific Costing
Setup
Standard Costing
Setup