Overlapping Operation Processing - APS
This topic applies only to APS.
You define overlap on an operation to represent the number of run hours 
 the previous operation must complete before this operation can start. 
 The system moves back the operation's start and end dates to reflect this 
 overlap. It then makes further adjustments to the operation's dates based 
 on the following circumstances:
	- Considers that the first operation may split across breaks for 
	 other operations (as defined in the Break 
	 Rule for the operation) and makes the necessary adjustment.
- Ensures the second operation does not end before the first operation. 
	 If the difference between the second operation's new start date/time 
	 and the end of the first operation is greater than the total duration 
	 of the second operation, the system adjusts the horizon again so the 
	 second operation cannot finish before the first operation.
If you run the Scheduler after running APS Planning, the Scheduler performs 
 its overlap processing based on the same Offset value.
Related Topics
APS Overview
APS Steps
Defining 
 Overlapping Operations
Current Operations
Defining 
 Overlapping Operations
Overlapping 
 Operation Processing - Scheduler