Adding Routing/Bill of Material Information Manually
This topic describes how to add a routing and bill of material to inventory 
 items (the current routing), jobs, production schedules, or estimate jobs.
NOTE: You can also 
 use the Engineering 
 Workbench form to create and maintain routing/bills of material.
Creating the Routing
	- Open the appropriate operations form: 
	
- Open the item, job, or production schedule to which you want to 
	 add an operation.
- Select Actions > New. - NOTE: Required 
	 fields are highlighted in a different color on the form. For a description 
	 of a particular field, right-click on the field on the form and choose 
	 Help. 
- Select the Standards tab (if not already displayed). The 
	 Standards tab defines operation setup, queue, and run times, as well 
	 as the start and end date. Enter data in the appropriate fields.
- Select the Resources tab. This tab defines the crew or machine 
	 resource groups that this operation requires in order to be processed, 
	 as well as parameters related to the resource groups. Enter data in 
	 the appropriate fields.
- Select the Costs tab. The only values you must enter are 
	 the Setup and Labor Run Rates, which are used in costing the operation. 
	 The Efficiency field is used for planning, scheduling, and costing.
- Select Actions > Save to save the operation.
Adding Materials
	- On the operations form, click the Materials button to add 
	 materials to the operation, if needed. This button opens the appropriate 
	 materials form: 
	
- Select Actions > New to add the new material.
- Enter the data in the appropriate fields.
- Select Actions > Save to save the new materials.
You can now release 
 the job or production schedule.
Related Topics
Creating 
 Routings and Bills of Material
Engineering 
 Workbench